Please use the navigation above to learn more.
SWRate Pro software is electrical rating software that calculates resistance, reactance, and thermal ratings in accordance with current standards. SWRate Lite software is available as a no-cost “lite” version of the SWRate Pro software. Each software includes an extensive database of overhead conductors and cables. SWRate software will calculate, for a specific set of input conditions:
No matter what question or concern you have about Southwire’s SWRate Pro software, we can help. You can Contact Us or reach us between the hours of 9:00 A.M. to 4:00 P.M. on Monday-Friday at 1-877-797-2410.
Welcome to SWRate Software!
SWRate software can be downloaded here.
SWRate Lite software is available as a no-cost “lite” version of the SWRate Pro software. SWRate software will calculate, for a specific set of input conditions:
SWRate Pro software is an advanced version and can be purchased here.
Southwire’s SWRate software was designed to run on the Windows® operating system.
*Windows is a registered trademark of Microsoft Corporation in the United States and other countries.
For SWRate software, you will find a link to the User’s Manual below.
The Installation Guide provides detailed instructions for installing SWRate software and registering a license.
In addition to the following links, the EULA and Maintenance Agreement can also be accessed in the software.
SWRate Lite is a limited functionality version and is available here: Download SWRate Pro. Once SWRate Lite is downloaded, a product key for SWRate Pro may be entered in order to easily upgrade your program.
We have many new features planned for future versions of SWRate Pro. New features include but are not limited to: adding a CIGRE calculation method option, adding a CSA strand factor option, additional conductor types, core temperature gradient calculations, ACSR strength options, and Metric unit display on the main menu.
Custom upgrades are available. Call sales support at 1-877-797-2410 – Option 1.
Yes. Please call sales support at 1-877-797-2410 – Option 1.
Call 1-877-797-2410 – Option 1 or use Contact Us.
No.
Call 1-877-797-2410 – Option 3.
Click on Help => About from the Main Menu.
The software may look different based on your monitor resolution. If you are having problems reading screens, please set your monitor to a lower resolution.
Contact your conductor supplier for information on conductors not listed in the conductor database. To add a custom conductor, use either the “Custom” Type or Edit Conductors feature. Please refer to the User’s Manual for more information.
Call technical support at 1-877-797-2410 – Option 3.
If an internet connection is not possible, please contact us at 1-877-797-2410 – Option 1 for additional licensing options.
Southwire’s SWRate software was designed to run on the Windows® operating system.
*Windows is a registered trademark of Microsoft Corporation in the United States and other countries.
Southwire has the trained experts to help you find the right product or solution!